News Center
Low-Profile Direct Drive Motor Provides Direct Control with Accuracy of a Servo Motor
Vernon Hills, Illinois - January 24, 2019
Machine designers and end users looking for direct control of a load without traditional transmission components will be interested in the new Low-Profile Direct Drive Motors (TM-RG2M / TM-RU2M) from Mitsubishi Electric Automation, Inc. Built with speed and precision in mind, it provides a smaller footprint and allows for more compact, efficient, and precise machines than those typically built using rotary servo motors. Applications that are well suited for the new motor include coating and vapor deposition systems, index tables, tool changers, rotary material handling robots, and rotary axis on XYθ inspection positioning systems.
Unlike rotary servo motors that are coupled to a load with a mechanical transmission such as a gear, coupling, or belt, the TM-RG2M / TM-RU2M Low-Profile Direct Drive Motor is coupled directly to a load, resulting in greater positioning accuracy, reduced energy use and less maintenance. It is ideal for use in industries such as semiconductor / LCD manufacturing, machine tool, material handling and inspection.
The new direct-drive motor allows users to reduce installation space, while combining direct control with the accuracy of a servo motor. It also allows for flexibility when sizing by allowing for compatibility with larger-capacity servo amplifiers such as Mitsubishi Electric’s MR-J4-40B (-RJ) with the TM-RG2M/TM-RU2M 004E30 to further increase torque. It features two installation methods – flange type with pilot and table type with positioning pinholes.
“The TM-RG2M / TM-RU2M Low-Profile Direct Drive Motor reduces the complexity of traditional mechanical power transmission systems which increases the machine efficiency and reduces downtime/maintenance by eliminating mechanical components,” said Dan Zachacki, Senior Product Marketing Engineer at Mitsubishi Electric Automation, Inc. “It provides customers with the all advantages of a servo motor in a compact package that is capable of supporting and driving a load directly.”
Additional information on the TM-RG2M / TM-RU2M Low-Profile Direct Drive Motor is available here.
— About Mitsubishi Electric Automation, Inc.
Headquartered in Vernon Hills, Ill., Mitsubishi Electric Automation, Inc. is a U.S. affiliate company of Mitsubishi Electric Corporation. It offers a broad product portfolio including programmable automation controllers (PAC), programmable logic controllers (PLC), human machine interfaces (HMI), variable frequency drives (VFD), servo amplifiers and motors, control software, computerized numerical controllers (CNC), motion controllers, robots and low-voltage power distribution products. Additional information about Mitsubishi Electric Automation is available at us.mitsubishielectric.com/fa/en/.
— About Mitsubishi Electric Corporation
With more than 100 years of experience in providing reliable, high-quality products, Mitsubishi Electric Corporation (TOKYO: 6503) is a recognized world leader in the manufacture, marketing, and sales of electrical and electronic equipment used in information processing and communications, space development and satellite communications, consumer electronics, industrial technology, energy, transportation, and building equipment. Mitsubishi Electric enriches society with technology in the spirit of its “Changes for the Better.” The company recorded a revenue of 5,003.6 billion yen (U.S.$ 37.3 billion*) in the fiscal year ended March 31, 2023. For more information, please visit www.MitsubishiElectric.com.
*U.S. dollar amounts are translated from yen at the rate of \134=U.S.$1, the approximate rate on the Tokyo Foreign Exchange Market on March 31, 2023
— About Mitsubishi Electric Factory Automation Business Group
Offering a vast range of automation and processing technologies, including controllers, drive products, power distribution and control products, electrical discharge machines, laser processing machines, computerized numerical controllers, and industrial robots, Mitsubishi Electric helps bring higher productivity – and quality – to the factory floor. In addition, our extensive networks around the globe provide direct communication and comprehensive support to customers. The global slogan "Automating the World" shows the company's approach to leverage automation for the betterment of society, through the application of advanced technology, sharing know-how and supporting customers as a trusted partner.
For more about the story behind "Automating the World" please visit: www.MitsubishiElectric.com/fa/about-us/automating-the-world
— About e-F@ctory
e-F@ctory is Mitsubishi Electric's integrated concept to build reliable and flexible manufacturing systems that enable users to achieve many of their high speed, information driven manufacturing aspirations. Through its partner solution activity, the e-F@ctory Alliance, and its work with open network associations such as The CC-Link Partners Association (CLPA), users can build comprehensive solutions based on a wide ranging "best in class" principle.
In summary, e-F@ctory and the e-F@ctory Alliance enable customers to achieve integrated manufacturing but still retain the ability to choose the most optimal suppliers and solutions.
*e-F@ctory, iQ Platform are trademarks of Mitsubishi Electric Corporation in Japan and other countries.
*Other names and brands may be claimed as the property of others.
*All other trademarks are acknowledged
— Media Contact
Pam Summers
Marketing Communications Manager
Mitsubishi Electric Automation
Pam.Summers@meau.com
+1 (847) 478-2415